Part Number: SN6505B
Hi all
Would you mind if we ask SN6505B?
<Question1>
Do you have any application in case of using external clock?
As the background of the this question, our customer would like to configure high frequency to reduce trans size with external clock.
<Question2>
If you have the formula which to calculate the value of inductance, could you give us the reference?
We would like to know relational expression between L and Fsw.
And then, the customer's condition are follows;
-Input voltage : 3.3V
-Output voltage : 3.3V
-Output current : more than 400mA
Kind regards,
Hirotaka Matsumoto