Part Number: ISO1050
Hi
How do i interpret ISO1050DW installation classification into UL 60950-1 Table 2N. Which population degree and material group on UL 60950-1 Table 2N should i refer to? thanks!
UL 60950-1 Table 2N
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1050
Hi
How do i interpret ISO1050DW installation classification into UL 60950-1 Table 2N. Which population degree and material group on UL 60950-1 Table 2N should i refer to? thanks!
UL 60950-1 Table 2N
Hi,
You should refer to Material Group II under 'Other Materials' tab. All of our testing is done based on Pollution Degree 2 but it really depends on your end application use. Are you planning to use the equipment under Pollution Degree 1, 2, or 3 environment? Depending on your end use, you can use the appropriate column in the Table 2N.