Part Number: TFP410
Hi!
We use the TFP410 ( TI PanelBus Digital Tansmitter ) for a DVI Interface.
We want to use the differential clock (LVDS) for IDCK+ and IDCK-.
The clock source is a XILINX FPGA.
QUESTION:
- Do we need an external termination resistor or is there an internal termination resistor available? ( 100Ohm? )
I didn’t find the information in the datasheet. - Should we use capacitive coupling of the clock signal with serial capacitor both in IDCK+ and IDCK- signal?
If yes, what capacitance is recommended ( 10nF or 100nF 0402)?
Thanks a lot,
Marcus