Part Number: TMDS181
Dear Team,
our customer would like to implement a functionality that allows the system to wake up when a HDMI signal is coming in.
Goal is to let the system be in a standby mode (<0.5W power consumption) and as soon as an active video signal is applied, somehow an interrupt should be generated.
The TMDS181 has an Input Signal Detect Block which is enabled via pin / I2C. But can we also use this block to generate a wake-up interrupt - independent of the FPGA of the system?
Looking forward to your feedback.
Best Regards
Martin