Part Number: TPS25740
Other Parts Discussed in Thread: TPS2514A
Hello,
The USB Power Delivery Specification Revision 2.0, Version 1.3 defines pinout and requirements for using USB Power Delivery with a Standard-A Connector (See Section 3.2.3).
The spec defines a 13-pin Standard-A connector with two "PD Detect" Pins and two "Insertion Detect" pins:
1) Does TI have a USB PD charging controller that can work with a USB 2.0 PD Standard-A Connector?
2) Do PD Detect pins use the same protocol as the CC pins in Type-C? Ultimately we want to connect iPad Pro 12.9" devices to USB-PD, but we must use Standard-A connectors. We can build out own USB 2.0 PD to Lightening if the signals are compatible.