This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there any chip that can do USB port detection



Hi Ti,

I am design an device which is powered by USB power adapter. My device operates in 5V 600mA. However, some USB adapter can provide 5V 1A power only with USB port detection. Therefore, is there any type of chip in Ti can do the detection? The following photo shows the design I want. 

Thanks for the help.

Ryan