This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB564: Active vs Passive USB Demux?

Part Number: TUSB564
Other Parts Discussed in Thread: HD3SS460,

I'm designing a system to run DisplayPort and USB 3.0 simultaneously over USB-C, both at 5 Gbps, and wondering what the advantages of an active switch like the TUSB564 compared to a passive switch like the HD3SS460. The TUSB564  is higher cost and higher power, but I assume the signal integrity is better? In what situations is the active switch required, or recommended?