Part Number: TUSB321
Hello,
Using TUSB321, UFP, what happens to DIR output pin when a voltage level within the proper threshold is detected on CC1 and CC2 at the same time.
Avinoam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB321
Hello,
Using TUSB321, UFP, what happens to DIR output pin when a voltage level within the proper threshold is detected on CC1 and CC2 at the same time.
Avinoam
Hi,
It's not possible to have a connection on both CC pins. The Type-C cable only has a single CC wire.
Regards,
Brian
Hello,
We have an option to connect our device directly , without cable, to a smartphone type C connector. In this case, I think two CC signals exist. How would TUSB321 perform. What would be on DIR pin.
Thank you,
Hi, that is not a valid configuration. If your device has a Type-C receptacle, then it must be connected via a cable or dongle (only 1 CC wire to the other side). If your device has a Type-C plug, then only 1 CC wire should be connected to the TUSB321 as the orientation is fixed and DIR is irrelevant. Either way, you can only 1 CC wire connected to the port partner. Please refer to the Type-C specification for further info.
Regards,
Brian