Hi team,
I tried transfer by "Line-Interleave Forwarding mode" the following "Test conditions".But, UB954.TX signal is no change.
Q.Are there other required register settings?
[Test condition]
1. Transfer Color-Bar-Pattern from UB953 to UB954.RX0.
2. Transfer Color-Bar-Pattern from UB953 to UB954.RX1.
3. Set UB954 to "CSI output:enable" & "CSI lane count :4lane"
4. Set UB954 to "Line-Interleave Forwarding" mode.
5. Set UB954 to "Forwarding enabled for RX Port 1" & "Forwarding enabled for RX Port 0"
[note]
In case of "Best-Effort CSI-2 Forwarding" , UB954.TX signal is change.
best regards.