This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6408A: High Level at the condition of "High than 3V"

Part Number: TCA6408A


Hi Team,

I plan to use the I/O extender of "TCA6408A" to detect the Photo-INT sensor which require at the codition of "the output level higher than 3V" .

Did anyobne have best -fit design for this requirement except to add the "INVERTER" before the I/O pin ? 

  • Hey Jackie,

    Could you provide a block diagram and maybe the device number of the photo sensor? (please provide Vcci and Vccp voltages as well )

    I am a little confused about this question and I am not sure if you are asking if there is a way to make the TCA6408A ViH higher than 3V (in this case our port would be an input) or if you are trying to make the sensor see something higher than 3V (you want to use TCA6408A port as an output).

    Thanks,

    -Bobby

  • Hi Jackie,

    Do you have any feedback on Bobby's questions above? Once we are able to better understand what is needed then we can propose a more specific solution.

    Regards,
    Max
  • Hi Jackie,

    Just checking in again - do you have any feedback on our questions? Or, is there any other way we can help?

    Max