This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1: Some questions about GPIOs of DS90UB949-Q1 with DS90UB948-Q1.

Part Number: DS90UB949-Q1
Other Parts Discussed in Thread: DS90UB948-Q1

Dear  All

       I will use DS90UB949-Q1 for Serializer, and use DS90UB948-Q1 for Deserializer.

       1.Configured the GPIO0 (14pin) of UB949 to output, configured the GPIO0 (7pin) of UB948 to input. If the high voltage signal send to the GPIO0 of UB948, the GPIO0 of UB949 will output high voltage ?without any software configuration ?

       2.The GPIO0 of UB949 corresponds to GPIO0 of UB948 ? The GPIO1 of UB949 corresponds to GPIO1 of UB948 ?  Can I configure GPIO0 of UB949 corresponds to GPIO1 of UB948 by configured the register ?

       3. For the D_GPIO[3:0] and GPIO[3:0], can I conclude that there are just supported different speed, and other functions are same?

       4. The GPIO_REG[5:8] only read by configured the register ?