This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: SN65DSI86 Link Training Issue

Part Number: SN65DSI86

I am trying to enable the color bar using the display port of the SN65DSI86. (I am using an ASUS monitor through a display port to HDMI converter). However semi auto link training is failing with 0xF8=0x02 and the monitor remains black. I have tried writing the registers exactly as given in the example (Typical Application 1080p panel) in the SN65DSI86 bridge documentation (additionally writing to the color bar and other related registers). If anyone has any sample code that does this or has any insight on this please share!

The addresses and data that i am writing are given below in order, 

address  =  { 0x0a, 0x10, 0x12, 0x5a, 0x93, 0x94, 0x0d, 0x95, 0x64, 0x74, 0x75, 0x76, 0x77, 0x78, 0x96, 0x20, 0x21, 0x24, 0x25, 0x2c, 0x2d, 0x30, 0x31, 0x34, 0x36, 0x38, 0x3a, 0x5b, 0x3c, 0x5a, 0x96}

data        =  { 0x06, 0x26, 0x59, 0x05, 0x20, 0x80, 0x01, 0x00, 0x01, 0x00, 0x01, 0x0a, 0x01, 0x81, 0x0a, 0x80, 0x07, 0x38, 0x04, 0x2c, 0x00, 0x05, 0x80, 0x94, 0x24, 0x58, 0x04, 0x00, 0x10, 0x0d, 0x01}

(I am waiting for the PLL to lock)

Monitor info is given below,

Monitor

 Model name............... ASUS VP228

 Manufacturer............. Asus

 Plug and Play ID......... ACI22C3

 Serial number............ H9LMTF143814

 Manufacture date......... 2017, ISO week 38

 Filter driver............ None

 -------------------------

 EDID revision............ 1.3

 Input signal type........ Analog 0.700,0.000 (0.7V p-p)

 Sync input support....... Separate

 Display type............. RGB color

 Screen size.............. 480 x 270 mm (21.7 in)

 Power management......... Active off/sleep

 Extension blocs.......... None

 -------------------------

 DDC/CI................... Supported

 MCCS revison............. 2.1

 Display technology....... TFT

 Controller............... Mstar 0x1600

 Firmware revision........ 0.1

 Firmware flags........... 0x00FF005A

 Active power on time..... 65535 hours

 Power consumption........ 6.55 kWh

 Current frequency........ 67.50kHz, 60.00Hz

Color characteristics

 Default color space...... Non-sRGB

 Display gamma............ 2.20

 Red chromaticity......... Rx 0.635 - Ry 0.352

 Green chromaticity....... Gx 0.321 - Gy 0.633

 Blue chromaticity........ Bx 0.151 - By 0.052

 White point (default).... Wx 0.313 - Wy 0.329

 Additional descriptors... None

Timing characteristics

 Horizontal scan range.... 24-83kHz

 Vertical scan range...... 50-75Hz

 Video bandwidth.......... 170MHz

 CVT standard............. Not supported

 GTF standard............. Not supported

 Additional descriptors... None

 Preferred timing......... Yes

 Native/preferred timing.. 1920x1080p at 60Hz (16:9)

   Modeline............... "1920x1080" 148.500 1920 2008 2052 2200 1080 1084 1089 1125 +hsync +vsync

Standard timings supported

    720 x  400p at  70Hz - IBM VGA

    640 x  480p at  60Hz - IBM VGA

    640 x  480p at  67Hz - Apple Mac II

    640 x  480p at  72Hz - VESA

    640 x  480p at  75Hz - VESA

    800 x  600p at  56Hz - VESA

    800 x  600p at  60Hz - VESA

    800 x  600p at  72Hz - VESA

    800 x  600p at  75Hz - VESA

    832 x  624p at  75Hz - Apple Mac II

   1024 x  768p at 60Hz - VESA

   1024 x  768p at 70Hz - VESA

   1024 x  768p at 75Hz - VESA

   1280 x 1024p at  75Hz - VESA

   1920 x 1080p at  60Hz - VESA STD

   1680 x 1050p at  60Hz - VESA STD

   1440 x  900p at 60Hz - VESA STD

   1280 x 1024p at  60Hz - VESA STD

   1280 x  960p at 60Hz - VESA STD

   1280 x  720p at 60Hz - VESA STD

   1152 x  864p at 75Hz - VESA STD

Report information

 Date generated........... 8/20/2018

 Software revision........ 2.90.0.1020

 Data source.............. Real-time 0x1300

 Operating system......... 10.0.10240.2

Raw data

 00,FF,FF,FF,FF,FF,FF,00,04,69,C3,22,C6,31,02,00,26,1B,01,03,68,30,1B,78,2A,84,D5,A2,5A,52,A2,26,

 0D,50,54,BF,EF,00,D1,C0,B3,00,95,00,81,80,81,40,81,C0,71,4F,01,01,02,3A,80,18,71,38,2D,40,58,2C,

 45,00,DC,0C,11,00,00,1E,00,00,00,FF,00,48,39,4C,4D,54,46,31,34,33,38,31,34,0A,00,00,00,FD,00,32,

 4B,18,53,11,00,0A,20,20,20,20,20,20,00,00,00,FC,00,41,53,55,53,20,56,50,32,32,38,0A,20,20,00,55