Part Number: DP83867ERGZ-S-EVM
Hello Team,
I have a design using the DP83867ERGZ and have a few questions - searching through other e2e posts I believe I found answers to a few questions but wanted to check with you all first.
- Which power is for the PHY to transformers – VDDIO, VDDA2P5, or VDDA1V0? Is it VDDIO?
- Datasheet and Eval board Users guide are inconsistent with decoupling caps – datasheet says10 nF cap, eval board shows 1nF cap. Which one is correct?
- In 10Base-T/100Base_Tx, what do I do with TD_A_P/N, and TD_B_+/N? TD_C_P/N and TD_D_P/N are connected to transformers (TX+/-, Rx+/-).
- No unused pins have special termination requirements
- Figure 20 in datasheet says: I need to strap resistors for RX_D[0:3]. But, I didn’t see that in the eval board user’s guide. What should I do?
- Strap pins have internal 9k ohm pull-down resistors. It is not required to add external pulls, but some people still do it for good practice.
- If I use only the SGMII interface (that is, SGMII_SI[P/N], SGMII_SO[P/N]), what do I do with the rest MAC interface pins?
Thank you!