Part Number: SN75LVCP600
Zdiff=80-115Ohm,does it mean the differential impedance shall be controlled to 85-115Ohm,including the tolerance of +/-10%?Or the difference impedance can be 85Ohm+/-10%?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75LVCP600
Zdiff=80-115Ohm,does it mean the differential impedance shall be controlled to 85-115Ohm,including the tolerance of +/-10%?Or the difference impedance can be 85Ohm+/-10%?
The receiver differential input impedance is specified to be between 85 and 115 Ohms. This device is typically used in applications which specify a transmission line impedance of ~ 100 Ohms. For SATA applications I would recommend to control PCB and cable impedances to 100 Ohms +/- 10%.
Regards,
Lee