Other Parts Discussed in Thread: TFP410, DS90CR288A
Hi,
I have two questions:
1. I have parallel connections coming in from a group of 16 photon counting modules (these are TTL pulses), which I would like to count and make a stats. I would like to connect these to a PYNQ board, which has a HDMI input, directly interfaced to the FPGA banks. Is it possible (even theoretically) to use TFP410 (or other similar ICs) to take 16 parallel inputs from the counting modules, and connect it to the FPGA through the HDMI port ? Has anyone tried this before ? I can do the decoding of the signal on the FPGA.
2. I also have a high speed camera (using cameralink) with a clock rate of 75 MHz. I would like to convert this to HDMI. For this:
Cameralink-Connector ->DS90CR288A -> TFP410 -> HDMI connector
Is the above a valid scheme ?
Thank you,
Mugundhan