Part Number: TVS3300
Hi,
Can TVS3300 be usd for EFT IEC 61000-4-4 Protection/Suppression. I have 18-30V DC Input.(24@2A current drawn by system under normal condition).
EFT pulses will be 5/50ns 15ms period with duration of 300ms for about 1 minute as per IEC standard.
TVS 3300 data sheet shows it can withstand 4A Current at (10/1000 µs)?
Is the power rating of TVS 3300 sufficient for EFT compliance. I want to replace SMCJ33A ( Clamping voltage of SMCJ33A is higher for my downstream electronics) with TVS 3300
Regards,
Sanjeev