Part Number: TSB81BA3E
Other Parts Discussed in Thread: TSB12LV01B,
Hi team:
My customer had problems with the TSB81BA3E and TSB12LV01B.
Using transformer coupling, the TSB81BA3E is configured in 1394A-only mode for the following two tests:
1). 2 channels LKON/DS2 through pull-up resistor to 3.3V, BMODE is grounded, PINT output (terminal 1) is not connected, LCLK_PMC input (terminal 7) is pulled up to 3.3V through pull-up resistor;
But finally they cannot be connected
2). 2 channels DS0 are grounded, BMODE is grounded, PINT output (terminal 1) is not connected, LCLK_PMC input (terminal 7) is grounded;
They are normally connected, but cannot be connected to 200M, 100M 1394 devices. View TSB81BA3E register This port is identified as beta mode.
Thanks for your help!