Hi,
Can you show me the reference schematic of Line-to-Line protection by ESD314 for RJ45? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
If you want line to line protection only, float the ground pin of the device. However, the device will provide line to line and line to ground protection if implemented in the way that the data sheet says.
Also if this in in an Ethernet application and you want to use the device between the connector and the transformer you cannot connect the ground pin as the common mode voltage can be too high on that side.
If the device is between the transformer and the phy, the ground pin can and should be connected for both line to line and line to ground protection.
If this is the same application that you have emailed me about then we can take this back on email if you need more details.