Part Number: DP83867IS
Hello,
My customer will be using the DP83867 with this RJ45+Transformer: https://belfuse.com/resources/StewartConnector/0826-1A1T-23-F.pdf
Do they need to split the ground planes and connect the planes together with two 1000pF, 2kV cap as shown in figure 36?
I ask because I noticed their connector has a 2kV capacitor already integrated. What's integrated in this connector looks just like the circuitry in figure 26.
What should we recommend:
- Still create a split ground and add two more 2kV capacitors like Figure 36 in the datasheet?
or - Simply connect the shield of the connector to ground since it already has a 2kV capacitor like Figure 26 in the datasheet?
Also, can two side-by-side RJ45 connectors share the same chassis ground?
Thank you,
Ryan B.