Part Number: DP83867IR
Hi all
Would you mind if we ask DP83867IR?
<Question1>
If we access followings address(registers higher than 0x1F), does it require to use clause 45 format? or clause 22 format?
-8.4.2.1.7 Example of Read Operation Using Indirect Register Access
-8.4.2.1.8 Example of Write Operation Using Indirect Register Access
<Question2>
We would like to confirm the op code in case of "Using Indirect Register Access" as follows;
8.4.2.1.7 Example of Read Operation Using Indirect Register Access
Read register 0x0170.
1. Write register 0x0D to value 0x001F : OP=01 ??
2. Write register 0x0E to value 0x0170 : OP=01 ??
3. Write register 0x0D to value 0x401F. : OP=01 ??
4. Read register 0x0E. : OP=11 ??
The expected default value is 0x0C10.
8.4.2.1.8 Example of Write Operation Using Indirect Register Access
Write register 0x0170 to value 0x0C50.
1. Write register 0x0D to value 0x001F. : OP=01 ??
2. Write register 0x0E to value 0x0170 : OP=01 ??
3. Write register 0x0D to value 0x401F. : OP=01 ??
4. Write register 0x0E to value 0x0C50. : OP=01 ??
Is our recognition correct?
Kind regards,
Hirotaka Matsumoto