Part Number: TPS65982
Other Parts Discussed in Thread: TPS65987D
Hello,
I have the TPS65982-EVM and the Aardvark i2c/spi host adapter. I am trying to understand the Application Customization Tool and am running into some problems. It looks like I get a successful hardware connection to i2c address 0x38 (SDA1/SCL1). I have followed the slva786a and slvuar8a PDF's and am still confused as to how this is working. I have my aardvark hooked up to the TPS65982-EVM the same way it is shown in the slva786a PDF. When I create a new project, and try to import the settings from the TPS65982-EVM, it says that it will go to the device 1, port 0 tab which is not viewable unless I'm in debug mode.. If i import the settings to the "Shared Device Settings", i see that registers in the "Common Settings" tab under "Raw View" are updated. There is no "Global Device Settings Tab" in my software that I can see. Also, if I set the I2C Address to 0x38 and perform a test read, it returns APP.
Is there an updated applications note for the newest Application Customization Tool?