Part Number: DS80PCI402
Hi,
We are using the DS80PCI402 in our design. We are operating the DS80PCI402 in master mode by keeping the ENSMB flaoting.
When the board is powered up and either EEPROM is blank or the first byte data is 0xFF , then there is continuous Smbus access happening to read the EEPROM.
If the EEPROM is programmed with configuration data, then repeater reads the EEPROM and stop the SMbus access after loading the configuration.
Is it the expected behavior for continuous SMBus access when the EEPROM is blank or first byte is oxFF?
Another issue is that EEPROM first bytes (0-4) get corrupted sometimes, can the repeater corrupt the EEPROM while doing the read access?
I have checked the I2C timings, it is meeting the spec as given in datasheet.
Regards,
Amit Mittal