To whom it may concern,
We require the LVDS outputs to be Hi-Z during the initialisation of the MIPI bridge.
From the datasheet it seems the only way to make the LVDS Hi-Z is as follows:
- De-assert the EN signal
-> This prevents the I2C commands from acknowledging when configuring the CSR at initialisation
- Entering ULPS
-> This is entered by transitioning the input MIPI signals to LP00 state, which is contrary to the required LP11 state when initialising
Please confirm if there is alternative way or workaround that allows to make LVDS Hi-Z during initialisation.
Many Thanks,
Bhav