Part Number: DP83848K
When the docking terminal with 83848k is set to 10M full duplex mode and 83848 to self-negotiation mode, is the negotiation result 10M half-duplex mode?
2. When the docking terminal with 83848k is set to full duplex mode of 10M 83848, 21, 22 feet are pulled down to the ground through resistance (the purpose is to set 10M full duplex), what is the working mode of 83848k in this case?
3, how to register 83848k into 10M full duplex by register?
4. When 83848k works in 10M half-duplex mode, whether the internal loop is returned, can not communicate with the rest of the port, how to remove the switch back through the register