Part Number: TCA9555
Dear Team,
I have a customer that used TCA9555 in expanding IO.
We get an issue on the scanning process.
Can you help us to clarify such question, thanks?
=========================
Stepping check: (Device address 0x20)
Script 1:
s1: power on DUT(Master)
s2: DUT sends scanning command which is 0x20 device address + "R" only to TAC9555 (Slave Device)
s3: Master Device gets NACK signal.
Script 2:
s1: power on DUT(Master)
s2: DUT sends formal READ 0x06 command, then Slave device returns 0xFF (correct).
s3: DUT sends scanning command which is 0x20 device address + "R" only to TAC9555 (Slave Device)
s4: Master Device gets ACK signal.
Best Regards
Kevin