Part Number: TCA9539
The minimal input rise time is 20 ns and the minimal input fall time is 20 x (VCC / 5.5 V) ns.
Are those specifications really correct for the SDA and SCL input terminals?
In the I2C-bus Specification, the minimal rise and fall time is the specification for the output terminals and the bus lines, and it does not seem to be the specification for the input terminals.
I2C-bus Specification, Version 6.0, 4th of April 2014
http://cache.nxp.com/documents/user_manual/UM10204.pdf
On our customer board, no problems have occurred but the minimal rise and fall time is approximately 2.4 ns. Is this minimal time allowed?
Best regards,
Daisuke