Part Number: TPD1E05U06-Q1
My customer has a problem with the polarity marking on the package of TPD1E05U06QDPYRQ1. A 'stripe' marks Pin 1 which is connected to IO while Pin 2 is GND. However he is measuring 0.78V from pin 1 to pin 2. Putting the device the other way round onto the board it behaves as expected, but then the stripe marking on the package would be wrong.
Any thoughts?
Best Regards
Josef