Part Number: TPS2544
Other Parts Discussed in Thread: TPS2549
My customer is concerned about the max output current. Now they are using TPS2544 for 3A continuous USB charging. But in datasheet, there's two descriptions. One I find in recommend operation conditions, Iout is 2.5A, another is Adjustable Current-Limit up to 3.0 A (typ), So my questions are,
1. If our device could support continuous 3A current output.
2. If not, any part in your team could support up to 3A.
3. If yes, according to the forum in the DS, Ios_ty=50250/16=3141mA, selecting 16K in the circuit, if it is ok FOR 3A charging?
4. In customer's application, they set CTL,CTL2,CTL3, ILIM_SET to 1111, If it is ok when power state is S3,S4,S5/
Thanks.