Part Number: TCA9617B
Other Parts Discussed in Thread: TCA9617A
Hi Team,
Customer is asking if VCCA 3.3V and pull up 5V setting can cause device damage risk for long term usage? Thanks.
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Francis,
Thanks for quick feedback.
I will try to understand the reason behind after reaching customer and update to you later.
I'm just curious, for TCA9617B, if pull up voltage 5V is higher than supply voltage 3.3V, could be any risk of damage. Please kindly check for me.
I thought, the internal ESD diode usually can survive below 10mA, pull up resistor of 4.7K ohms should be big enough to limit this current into device whenever over voltage happen, is it reasonable to you?
Thanks.
Andrew
I double checked. The TCA9617B is ok to do this. It doesn't have an ESD devices that can be back biased into Vcc under those conditions. The TCA9617A does and you would have be careful with that part if you did this. You are good to go with the TCA9617B.
-Francis