Part Number: USB-2-MDIO
Other Parts Discussed in Thread: MSP430F5529, DP83849I,
Dear All,
I want to set up a serial communication (LabView) via MSP430F5529 to the PHYTER Demo II Board with DP83849i.
Is there a possibility to replace the usb-2-mdio program with a serial terminal program, like hyperterminal or labview?
With the recommended syntax below for reading a register '=' 'PHY_ID[2]' 'REG_ADD[4]' '/' I got the answer-string: >Error! Improper length format in basic read/write<
I tried the following:
=010001/
=,0,1,0,0,0,1,/
'=','0','1','0','0','0','1','/'
Where is the mistake?
The UART-setup seems to be ok, I noticed a respond on the MSP430-Board when sending the command (red and green leds were on a short low level).
Thank You
Stefan