Part Number: TPS65983B
Other Parts Discussed in Thread: TPS65987D, TPS65987, TPS65982, TPS65988
Hello,
How do you support DisplayPort alt mode on the TPS65983b?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zach,
The TPS65983B is only to be used for TBT device designs following an Intel reference design. If this is not the case for your design, please use the TPS65987D. You can enable DP mode using the TPS6598x Application Customization Tool
If this answers your question, PLEASE select This resolved my issue
Thank you,
Eric
Eric,
What is the difference between DDH and DH for the TPS65987? Also, what are the main differences between the 87D and the 88? Does the TPS65987D have the same TPS65983B features?
Also, when using a TPS65982, I seem to be having troubles getting into TBT alt mode when interfacing with a HUB that uses Intel's TBT Reference design. Our product works fine when interfacing with an older TBT reference design which has a cactus ridge on board, but when plugging into the HUB or the Tapex Creek eval board, our product is not automatically entering TBT alt mode. Thoughts? I appreciate all of your help.
Thank You,
Zach
Hi Zach,
87D and 87DDH are the same part, no differences between them. The 87D is a single port PD controller with two integrated power paths. One is typically used for sourcing power and the other for sinking power. The TPS65988 is a dual port PD controller with two integrated power paths where the two internal power paths are used for sourcing power to each port. The TPS65988 and 87D also offer external GPIO control for a PFET power path.
What feature of the 83B are you specifically looking for? The TPS65987D has most of the same features as the 83B.
If this answers your question, PLEASE select This resolved my issue
Thank you,
Eric