Part Number: DS90C387
Other Parts Discussed in Thread: TFP401,
Hello
I'm working on a prototype for a large series (10k products in the firsts years) of audio-visual products, that includes an HDMI to LVDS Open LDI conversion between the CPU and the monitor. I have issues with video transmission on this product, that are critically blocking the prototyping phase and so the serial industrialization phases.
The solution that was chosen for this was coupling two TI chips, a TFP401 followed by a DS90C387 chip. The schematic was done according to those component's datasheets, typical applications and evaluation boards examples that I found, and I have been even more confident in my design after seeing a board similar already sold on the web (link). The wire between the board and the screen is quite short (about 20cm).
Though, during validation phases I'm facing an issue on the video transmission, and it appears that two LVDS channels aren't working on the output of DS90C387 chip, A0M/P and A1M/P. The voltage on those pins stays at about 2.5V for the A0M & A1M output and 0VS for A0P & A1P. I have looked into each signal on my video connector without having a screen connected and on those 4 tracks I see a quite constant voltage whereas I can see some signals looking like frames on A2P or A4M for example.
After several chips replacements and debug tests, I'm asking for some support because I don't know where to search now, there aren't so many configuration entry and even if I tried to change them slightly none of them seem to be related to this particular issue in chip description.
Thank you very much for your quick answer,
Regards,
Rémi