This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TLK10232: TLK 10232 Access via MDC and MDIO

Part Number: TLK10232


Tool/software: Linux

Hi All,

             We are facing a serious issue with respect to TLK10232. We made a customized design with T4240 Processor along with the TLK10232. We are using U-Boot version - 2016.01 and kernel version - 4.1.8 .  TLK10232 mdc and mdio are connected to the T4240 Processor.  Input reference clock is 156.25MHz. Pins That are hardwired,

PRTAD[4:0] - 11010,

ST - 0 and

MODE_SEL - 0

How can we able to perform the read and write operation on TLK10232 to achieve 10G . Bulk Production is on hold due to this issue. Kindly Provide some idea to resolve this issue.

Thanks in Advance.

Regards,

Avinash N