This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1540: ISO1540DR P2P MAX14933ASE+T

Part Number: ISO1540

Dear Team,

Do we have P2P solution to change MAX14933ASE+T?

I can only find ISO1540DR have similar performance but not P2P(pin to pin).

Best Regards

Kevin

  • Hi Kuan,

    Since the isolated I2C function only requires about 8-pins as also shown in MAX14933, TI only has 8-pin I2C device family - ISO154x.
    Since ISO1540 is going to provide space advantage over MAX14933, I believe one would prefer the ISO154x over the MAX14933.

    Is there any other concern does customer have in using ISO1540? Let me know, thanks.


    Regards,
    Koteshwar Rao