Part Number: DS90UB953-Q1
Hi,
an engineer needs to power a 2A load over a 15m cable.
1. Is that feasible?
2. are there recommendations that can be offered as far as filtering and countering potential ground lifting issues.
Thank you!
-Alberto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953-Q1
Hi,
an engineer needs to power a 2A load over a 15m cable.
1. Is that feasible?
2. are there recommendations that can be offered as far as filtering and countering potential ground lifting issues.
Thank you!
-Alberto
Hi Alberto,
Our POC network cannot handle 2A due to the current limit of the inductors.
What do you mean by ground lifting? If you have multiple ground layers with voltage potential between them, you can try to populate vias around the board to connect the ground layers.
Best,
Jiashow