This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO2001: PRST pin behavior

Part Number: XIO2001

Hello,

 

I have a question about /PRST pin behavior of XIO2001.

 

Now I have one XIO2001 device which may be broken or may have a kind of defect.

Then I have to investigate what happens to this device.

 

In this device, /PRST pin never goes to High even after /GRST is deasserted.

 

Then my question is that does /PRST pin go to HIGH without any action after /GRST is deasserted?

Or is any additional action required do have /PRST pin go to HIGH?

I would like to know whether there is any conditions to have /PRST pin go to high.

 

Regards,

Oba

  • Oba,

    I do not believe PRST goes high without any action after GRST goes high. Please see quote from data sheet on page 27 on one way to assert PRST.

    "When bit 6 (SRST) in the bridge control register at offset 3Eh (see Bridge Control Register) is asserted, the bridge asserts the PRST terminal. A 0 in the SRST bit deasserts the PRST terminal."