Part Number: DP83848C
Hello, everyone.
I've some issues on the ethernet phy device DP83848.
At speed 100mb/s (autonegociation), the green LED (LINK) blinks and never stays ON.
I think it means that the link is not established
At speed 10mb/s, everything work. the LINK LED stays ON and the pcb can get its ip address by DHCP.
I don't think that it's problem from the software.
Beause,even if there is nothing in the microcontroller, once we plug the RJ45 cable, the green LED should be light and stays ON.
I've downloader an CAN demo example into my demo board (MCB1700) and then I plug the RJ45 cable to the demoboard.
The link LED turns on immédiately even if the ethernet is not initialized.
But when I did the same thing with the PCB, the LINK LED blinked and never stays ON.
This problème is only detected on serveral PCB.
Do you have some idea about this problee?