This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DPHY440SS: How to use

Part Number: SN75DPHY440SS

Dear Sir/Madam,

I do not quite make sure whether this part could be used on our project.

Our camera module uses Samsung S5K3P3SQ.

I saw the switching characteristics of DPHY link on data sheet is 1Gbps max. and the HS clock input range is between 100MHz and 750MHz.

How do I know these spec. could fit the spec. of camera module?

I plan to place your chip near my APU, but I do not know how to set the resistors' value of four pins.

Do you have any procedure that I could refer to?

Thank you.

Regards,

Albert Tseng