Other Parts Discussed in Thread: TCA9545A,
Dear all,
If the control register of the TCA95444A is set at 0b00000000, does it reset the I2Cx (x=1,2,3,4) interfaces ?
If not, can the TCA9545A perform a reset when the control register is set at 0b00000000 ?
In the application I need to be sure to reset the I2Cx in case of slave fault, but I cannot use any extra pin (such as reset pin of TCA9545A).
regards,
Domenico