Part Number: TPD4S214
Hi Team,
My customer is looking for OVP & OCP device for USB OTG.
The requirement is the following.
- over voltage protection up to 28V VBUS
- OVLO (output overvoltage lockout) threshold is 6~7V
- current limit is adjustable more than 1.5A
There is TPD4S214 however current limit is up to 1.2A.
Is there another solution for this requirement?
Best Regards,
Yaita / Japan disty