This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9555: What is the I/O pin logic status when it powered on

Part Number: TCA9555


Hi,

I am using TCA9555 to drive some relay drivers, and like to know the I/O output status when it just powered on. The spec says the I/Os are configured as inputs, and the block diagram shows a 100K pull-up resistor to VCC. Can I assume that the I/O output status is default to high/VCC?

Thank you,

Ray