Part Number: SN75DPHY440SS
The MIPI CSI2 specification for the HS clock is 80 to 750Mhz. What happens to this part do if the MIPI clock frequency is between 80 and 99.9999999Mhz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75DPHY440SS
The MIPI CSI2 specification for the HS clock is 80 to 750Mhz. What happens to this part do if the MIPI clock frequency is between 80 and 99.9999999Mhz?
Hi David,
Thanks for the explanation on the DPHY specification. I was referring to the last paragraph of section 4.1 of the specification that reads "a bit range of 80 to 1500Mbps per Lane.". Maybe the SN75DPHY440SS part does not able to do de-skewing of the data lanes below 100Mhz. I would like to know what the part does below 100Mhz as it may still be applicable in the application I have as de-skew below the 100Mhz or 200Mbps is probably not necessary given the width of the eye pattern on the data relative to the clock.
Harry