Part Number: TLK2711-SP
I wanted to confirm the functionality of the RKMSB and RXCLK pins when the device is disabled (enable = L).
RKMSB
When the device is disabled, it looks like RKMSB will output the state of the LOS circuit, which looks like it's active low in this mode. So if there is no input on the RXP/RXN serial input lines, then RKMSB should drive low when the device is disabled, correct?
RXCLK
When the device is disabled, it looks like RXCLK goes to a high impedance state. Can you confirm?
Thanks!