Hi
I used SN75451B in my project , when I test the board ,the chip very hot ,please help to review my design ,is it have some mistake? Thanks a lot .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I used SN75451B in my project , when I test the board ,the chip very hot ,please help to review my design ,is it have some mistake? Thanks a lot .
Hi Chen Chen,
Do you have a bypass capacitor on VCC? The datasheet mentions adding a 0.1uF bypass cap to prevent power disturbances/glitches.
Are you tying the input 2 channel, pin3, to VCC or GND?
Which package of the SN75451B are you using? If you look at the thermal calculations, 65C seems reasonable. Since you're dissipating 5V @ 50mA, your average power dissipation is 0.25W. Looking at the thermal information on page 4, if you're using the D or PS package, you could be dissipating ~120C/W * 0.25W = 30C of heat, which would be similar to the 65C that you're measuring on the package.
Thanks,
Arthur Huang