Part Number: TCA9548A
Dear Team:
Programming TCA9548A issue: Whether can we program I2C by I2C BUS0..I2C BUS7?
Another questions: Input I2C bus (pin22,23) don't turn on, whether another I2C BUS0..I2C BUS7 can switching turn on to Pin22,23 I2C?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9548A
Dear Team:
Programming TCA9548A issue: Whether can we program I2C by I2C BUS0..I2C BUS7?
Another questions: Input I2C bus (pin22,23) don't turn on, whether another I2C BUS0..I2C BUS7 can switching turn on to Pin22,23 I2C?
Hello Thomas,
"Programming TCA9548A issue: Whether can we program I2C by I2C BUS0..I2C BUS7?"
-You can only program the device when it turns on by the main SDA/SCL pins. After you enable a channels, you could program the switch from the enabled channels but you could also disable the channel you are writing on...... I would recommend you always communicate to the device from the main channel.
"Another questions: Input I2C bus (pin22,23) don't turn on"
I don't understand. This is the main channel to the switch, all signals come of go through this channel. You have to program the device from this channel after you turn on the device.
-Bobby