Part Number: DS90UB954-Q1
Hello Sir,
I have some questions on DS90UB954-Q1.
1.Because 954 can support two channel input, can it support two different serialize IC, such as one is 913A with 720p 30fps, another one is 953 with 1080P 60fps?
2.If can support two different serialize, What specific requirements do you have?
3.If use the same serialize chips, the serialize can support different resolution and frame rate?
thanks!