Part Number: SN65HVD235
I didnt understand very well those statements:
"After transmission of an error frame, an error passive node must wait for 6 consecutive recessive bits on the bus before attempting to rejoin bus communications" (Microchip)
"Therefore, error-passive receivers shall always wait for six subsequent equal bits after detecting an error condition, until they have completed their error flag" (ISO 11898-1)
"The error passive station waits for six consecutive bits of equal polarity, beginning at the start of the passive error flag. The passive error flag is complete when these 6 equal bits have been detected" (CAN 2.0 Specification)
Could someone explain me that?
They're all telling about the same thing?