Part Number: TPS2546
Hi,
I have some question about STATUS pin behavior as below.
- What would be the possible STATUS behaviors under CDP mode? From the datasheet, I see 3 scenarios as below. May i know if there's any other scenario missing here? Can you explan the 2nd scenario? I don't fully understand the definition of "an attached device does a BC1.2 primary detection"
- STATUS asserts in CDP when load current is above ILIM_LO+60 mA for 200 ms.
- STATUS asserts in CDP when an attached device does a BC1.2 primary detection.
- STATUS de-asserts in CDP and DCP when the load current is below ILIM_LO+10 mA for 3 s
- I know STATUS is functional under 3 modes as described below (based on Table 3. Truth Table). DOes it mean STATUS is not functional at all the other modes?
- 0011(DCP_AUTO): Load Detect – Power Wake functionality.
- 0111(DCP_AUTO)): Load Detect – Power Wake functionality.
- 1111(CDP): As mentioned above
Thanks!
Antony