Other Parts Discussed in Thread: XIO2001
We have used XIO3130 PCIe switch in one of our design application. On downstream side, we have connected
three Wi-Fi modules.
The control pins for these modules (For Example, disable signal, clock request signal) are connected to the GPIOs
of XIO3130 switch. Upstream port is connected to NXP P1020 processor.
Can we drive these GPIO pins with software kernel running in P1020? and can we configure the state (input, output or float) of these GPIOs
through software or it has to be done through the EEPROM?
Thanks,
Dhaivat Master