This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9554: Asking for the TCA9554 schematic review

Part Number: TCA9554

Hi Team,
Customer would like to use TCA9544. Would you please review the schematic and provide your comment?


BR,
SHH

  • Hello SHH,

    Are all the ports going to be set as outputs? If not then it looks like they will be floating inputs, if they are being used as inputs then I would suggest you reference them to either GND or Vcc with a resistor.

    I assume you will have a pull up resistor on SDA/SCL/INT as I do not see them in the schematic.

    Lastly you may want to throw a capacitor on Vcc, something like 0.1uF should work.

    Thanks,
    -Bobby